General Info

Representing threads in technical drawings

The correct representation of threads in technical drawings serves as a basis for technical communication between participating trades. Extensive information can be presented in a clear and internationally understandable manner and thus supports the smooth process in mechanical manufacturing, production and assembly. In this article, you will learn how threads and bore holes are shown in detail in mechanical engineering.

8 Minutes read

Calculating shear strengths and tensile strengths for screws

Shear strength and tensile strength are two important parameters for selecting and using screws. Screws are used to connect components in a friction-locking manner and to withstand mechanical loads. In order to ensure that screws meet the required strength requirements in a given application, it is important to know what shear strength and tensile strength are and how they are calculated.

8 Minutes read

Understanding bearing damage – Causes, failure mode and prevention

Rolling bearings are robust and reliable components in mechanical engineering and custom machine construction. Under certain conditions, however, bearing damage to these widely used machine elements can occur, usually resulting from unusual behavior during operation. In the worst case, bearing damage can result in a complete failure of the rolling bearings, which can result in unwanted downtime. Therefore, it is important to detect the first signs of rolling bearing damage early on and to remedy their causes. In this article, we discuss the symptoms of bearing damage, its causes and typical failure modes.

10 Minutes read